AXIS#.SETUPREQLIST

Description

This parameter returns the list of parameters that must be set before the drive can be enabled and also whether or not each one of those parameters is set. This list of parameters will vary depending on the value AXIS#.MOTOR.TYPE. The drive can only be enabled when all commands have a value of 0.

Example

-->SETUPREQLIST

AXIS#.IL"Instruction list" This is a low-level language and resembles assembly.KP 0

AXIS#.MOTOR.ICONT 0

AXIS#.MOTOR.IPEAK 0

AXIS#.MOTOR.POLES 0

-->

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read Only

Units

N/A

Range

N/A

Default Value

N/A

Data Type

String

Stored in Non Volatile Memory

No

Variants Supported

All variants are supported

Related Topics

AXIS#.SETUPREQBITS , AXIS#.MOTOR.AUTOSET

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen